DOCA0096EN-02

Device Overview

Circuit Breaker and Switch-Disconnector Description

A Power connection (EverLink lug, EverLink lug with control wire terminal, compression lug / busbar, mechanical lug)

B Connection system cover

C SD presence indicator

D QR code to product information

E Termination information

F Product and accessory data labels

G Toggle handle

H Push-to-trip button

I Seal for setting cover

J Tripping curve

K DIN rail lock

L Current setting button (for circuit breaker only)

M Device identification, certification marks, and IEC/EN interrupting ratings

N MN or MX presence indicator

O OF presence indicator

P Seal for accessory cover

Earth-Leakage Circuit Breaker (ELCB) Description

A Power connection (EverLink lug, EverLink lug with control wire terminal, compression lug / busbar, mechanical lug)

B Connection system cover

C SD presence indicator

D QR code to product information

E Termination information

F Product and accessory data labels

G Toggle handle

H Push-to-trip button

I Seal for setting cover

J Trip unit

K Switch to isolate the device during dielectric tests

L DIN rail lock

M Device identification, certification marks, and IEC/EN interrupting ratings

N Test button of earth-leakage protection

O Earth-leakage trip indication

P MN or MX presence indicator

Q OF presence indicator

R Seal for accessory cover

The trip unit is described in a specific topic.

QR Code

Scan the QR code to get additional information about the circuit breaker from the Schneider Electric web site. To scan the QR code, use a smartphone that is equipped with a camera and installed with a QR code reader.

Accessories

The following accessories are available for the circuit breaker.

A Interphase barriers

B Long terminal shield

C Terminal spreaders

D Power distribution connectors (3-hole or 6-hole)

E Compression lug / busbar connector

F Aluminum mechanical lug

G EverLink lug without control wire terminal

H EverLink lug with control wire terminal

I Torque limiting breakaway bits

J Side rotary handle (right or left)

K Direct mounted rotary handle

L Extended rotary handle

M Open door shaft operator

N PowerTag Energy F160

O Wireless indication auxiliary

P OF or SD auxiliary contact

Q OF auxiliary contact pre-wired

R SD auxiliary contact pre-wired

S MN or MX voltage release

T MN undervoltage release pre-wired

U MX shunt trip pre-wired

V Fixed toggle handle padlocking device (OFF only)

W Fixed toggle handle padlocking device (OFF and ON)

X Removable toggle handle padlocking device (OFF only)

Y Rear insulating screen

Z SDx module (for earth-leakage circuit breaker only)

Sealing Accessories

The following sealing accessories can help prevent unauthorized changes to the circuit breaker.

Seal type

Helps to prevent

Seal image for circuit breaker

Seal image for earth-leakage circuit breaker

Seal for cover

  • Removal of the front cover

  • Access to the auxiliaries

Seal for long terminal shield

  • Access to the power connections (helps to prevent direct contact)

  • Dismounting of the circuit breaker

Seal for settings

  • Access to settings

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.