DOCA0096EN-02

Switch-Disconnectors

Introduction

A switch-disconnector is a control device that can be used to open and close a circuit under normal operating conditions. The switch-disconnector can make or break its rated current. For an overload or a short-circuit, it must be protected by an upstream device, in compliance with installation standards.

Switch-Disconnector Utilization Category

Depending on the rated operational current and the mechanical durability (A for frequent operation or B for infrequent operation), standard IEC/EN 60947-3 defines the utilization categories as shown in the following table. ComPact NSXm NA switch-disconnectors comply with utilization categories AC-21A or AC-22A up to 160 A and AC-23A up to 100 A.

Utilization categories

Infrequent operation

Frequent operation

Characteristics

AC-21B

AC-21A

Switching of resistive loads including moderate overloads (cos φ = 0.95)

AC-22B

AC-22A

Switching of mixed resistive and inductive loads, including moderate overloads (cos φ = 0.65)

AC-23B

AC-23A

Switching of motor loads or other highly inductive loads (cos φ = 0.45 or 0.35)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.