Voltage Releases
Characteristics
The following voltage release auxiliaries are operated remotely by an electrical trip command:
-
MX shunt trip
-
MN undervoltage release
-
MN undervoltage release with time-delay unit. The time-delay unit helps to overcome nuisance tripping due to transient voltage dips. The time delay is adjustable up to three seconds.
Voltage release auxiliaries are installed in the case under the front face of the circuit breaker. The presence and characteristics of a voltage release auxiliary are displayed through a window on the front face.
The characteristics of voltage release auxiliaries comply with IEC/EN 60947-2 recommendations.
|
Name |
Image |
Description |
|---|---|---|
|
MN undervoltage release |
Use this type of accessory for failsafe emergency stops. |
|
|
Time-delay unit for MN undervoltage release |
Removes nuisance tripping of an undervoltage release by setting a time delay of up to 3 s to overcome transient voltage dips. Adjustable and fixed time-delay units are available. |
|
|
MX shunt trip |
Trips the circuit breaker when the voltage exceeds 0.7 times the rated voltage (Un). NOTE: MX shunt trip 110/130 Vac combined
with Class I ground-fault sensing element
is suitable for ground-fault protection. In this application, the
circuit breaker trips when the voltage exceeds 0.55 times the rated
voltage (Un).
|