DOCA0096EN-02

Wireless Indication Auxiliary

Introduction

The wireless indication auxiliary provides remote and local information about the circuit breaker status.

The position of the wireless indication auxiliary inside the case, and the setting of the gateway or panel server, determine its function. The wireless indication auxiliary provides the following information remotely:

Position of wireless indication auxiliary Information provided

OF slot

Open/close circuit breaker status

SD slot

Trip indication

When in the SD slot, the wireless indication auxiliary can be configured to indicate a circuit breaker trip locally. The status LED blinks orange for eight hours.

The wireless indication auxiliary must be paired with a gateway or panel server.

The wireless indication auxiliary is powered by an internal battery. It sends a notification to indicate that the battery needs to be replaced.

For more information about installation, consult the instruction sheets on the Schneider Electric website: NNZ8881001 Wireless Indication Auxiliary Instruction Sheet

Description

A Reset button

B Status LED

C RF-Id identifier

D Actuator

E Battery cover

F QR code to access device information, including wireless address

Reset Button

The reset button allows you to :

  • Access setting mode to set the status LED indication mode

  • Pair or unpair the wireless indication auxiliary

Status LED

A status LED on the wireless indication auxiliary provides the following information:

  • Help with commissioning and maintenance steps

  • Status of communication between wireless indication auxiliary and gateway or panel server

  • Status of the wireless indication auxiliary

  • Indication of circuit breaker trip (available when LED indication mode is ON).

Status LED Description Action
Wireless indication auxiliary switched off or not currently in communication with gateway or panel server. None
Wireless indication auxiliary in pairing mode, searching for a gateway or panel server. Wait until the gateway or panel server is identified.
Wireless indication auxiliary in identification mode. Wait until wireless indication auxiliary is discovered in network.
Wireless indication auxiliary in communication. One green flash at each frame sent. None

Trip indication when wireless indication auxiliary is in SD slot and configured in LED indication mode ON

Check tripping cause.
Occasional loss of communication with the gateway or panel server. Check communication setting with the gateway or panel server.
Wireless indication auxiliary in setting mode, with LED indication mode set to OFF. Set LED indication mode to ON by pressing the Reset button.
Wireless indication auxiliary in setting mode, with LED indication mode set to ON. Set LED indication mode to OFF by pressing the Reset button three times in less than two seconds.

Flashes only when actuator is activated

Battery out of power Change the battery.

Commissioning

Commission the wireless indication auxiliary by using EcoStruxure Power Commission software or the webpages of the gateway or panel server.

NOTE: Check the firmware of the gateway before performing the commissioning of the wireless indication auxiliary. It is recommended to upgrade to the latest version available.

Step

Action

1

Put the wireless indication auxiliary in pairing mode in one of the following ways:

  • If the wireless indication auxiliary is not installed in the circuit breaker, press the reset button or the actuator.

  • If the wireless indication auxiliary is installed in the OF slot, open and close the circuit breaker.

  • If the wireless indication auxiliary is installed in the SD slot, open, close and action the push-to-trip button on the circuit breaker.

Result: The status LED blinks orange. The wireless indication auxiliary stays in pairing mode for three minutes.

2

Pair the gateway or panel server with the wireless indication auxiliary by using EcoStruxure Power Commission software or the webpages of the gateway or panel server.

Result: The status LED blinks green to indicate that the wireless indication auxiliary is paired.

3

Configure the wireless indication auxiliary by using EcoStruxure Power Commission software or the webpages of the gateway or panel server.

Setting LED Indication Mode

Set the LED indication mode of the wireless indication auxiliary to ON to indicate a trip locally when the wireless indication auxiliary is installed in the SD slot. The LED indication mode is factory-set to OFF.

Follow this procedure to change the LED indication mode.

Step

Action

1

Press the reset button.

Result: the wireless indication auxiliary wakes up.

2

Press the reset button three times in less than two seconds.

Result: The wireless indication auxiliary is in setting mode. the Status LED flashes three times every two seconds if LED indication mode is OFF, or six times every two seconds if LED indication mode is ON.

3

Press the reset button once to change the LED indication mode from OFF to ON, or from ON to OFF.

4

To exit setting mode, press the reset button for three seconds.

NOTE: If the reset button is not pressed, the wireless indication auxiliary exits setting mode after two minutes.

Replacing the Internal Battery

The wireless indication auxiliary sends a notification six months before the battery needs to be changed. For more information, see LVPED217032EN ComPact NSX & NSXm Catalogue.

Follow this procedure to replace the internal battery.

Step

Action

1

Remove the wireless indication auxiliary from its slot. Refer to Wireless Indication Auxiliary Instruction Sheet.

2

Remove the battery cover.

3

Remove the battery and recycle it.

4

Insert the new battery, following the guidelines marked in the battery compartment.

5

Put back the battery cover and lock it.

6

Reinstall the wireless indication auxiliary in its slot.

7

Put back the front cover of the circuit breaker.

Replacing the Wireless Indication Auxiliary

Follow this procedure to unpair the wireless indication auxiliary and delete it in EcoStruxure Power Commission software or the webpages of the gateway or panel server before replacing the wireless indication auxiliary.

Step

Action

1

Remove the wireless indication auxiliary from its slot. Refer to Wireless Indication Auxiliary Instruction Sheet.

2

Unpair the wireless indication auxiliary by pressing the reset button for at least three seconds and releasing, or by using EcoStruxure Power Commission software or the webpages of the gateway or panel server.

3

Install the new wireless indication auxiliary in its slot.

4

Pair the wireless indication auxiliary by following the procedure in Commissioning.

5

Put back the front cover of the circuit breaker.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.