DOCA0283EN-05

Maintenance Mode Filtering

Added filtering in Assets in maintenance tab.

You can filter by the following criteria:

  • Asset functional name: type the name of the asset in the box

  • Status: select a status from the options

  • Start or end date: set a date in one or other box to see events before or after the set date

Click the Apply Filter button to start filtering.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?