DOCA0283EN-05

Screens in OMD

The creation of the new asset type ClimaSys cooling unit has an impact on the following screens of the EAA web portal.

Overview Tab

In OMD, the Overview tab includes:

  • Temperature tracking and thresholds

  • Operating values from ClymaSys (last value and historical records)

  • Status:

    • Green: active

    • Grey: inactive

  • A chart with status history and records for Open door alarm

  • A chart displaying the Compressor number of cycles and the Condenser fan working hours

Asset Details Tab

For the new asset type ClimaSys cooling unit, there is a new typical layout for the Asset details tab, including partial health indexes.

Properties Tab

The Properties tab displays the main properties and attributes of the ClimaSys cooling unit asset type.

Insights Tab

In the Insights tab, it is possible to add a customized widget by selecting any of the new indicators created.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.