DOCA0283EN-05

Other Improvements

  • Related to the method to compute connection quality and temperature discrepancy for the three phases, monitoring level is now considering the whole information in a more consistent way to compute all items and assign monitoring level.

  • In the threshold pop-up window, the trends can now be added independently from the status being active.

  • For water freezing detection, a new rule identifies when ambient temperature drops below 0 ºC. This allows the user to identify the potential issues:

    • For facility in general.

    • For water based systems in particular, such as sprinklers and water pipes.

    In such a case, an alarm is triggered.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?