Improvements to EAA Web Portal
Improvements are available in EAA web portal. Ergonomic improvements provide a better user experience.
Fire Risk Index Renaming
The Fire risk index has been renamed to Fire index. No changes were made to the content or to the index calculation method.


Thermal Monitoring Tab
In the Thermal monitoring tab, a few improvements facilitate the access to the right information:
-
When selecting a position, the accordion menu opens, with the different temperatures values. It is possible to expand the view for the temperatures, which are sorted alphabetically.
-
The neutral phase temperatures are not displayed if there is no data recorded.
In the Thermal monitoring tab, in the Predicted temperature widget, the icon to analyze used to be displayed to all users. It is now limited to internal users (CSH and partner users).

LV Circuit Breaker Position in the Overview Tab
-
In the Overview tab, a new line has been included in the widget Operations and trips: the indicator Circuit breaker closed (Boolean type).
-
The information displayed is a green button when the circuit breaker is in the closed position.
-
By clicking on the value, the user can visualize the evolution of the indicator over time (functionality available for any indicator).

Electrical Health for Induction Motor
For the induction motor asset type, the Electrical health indicator has been renamed to Motor electrical health, to avoid confusion with other drive train components.