990-6139E-001

Connect Synchronization Cables Between Two UPS Systems (Option)

The maximum configuration is two parallel systems of four UPSs.
  1. Connect the optional synchronization cables between the UPS systems according to the concept below.

    Synchronization Cable Connection for Two Single UPSs

    Synchronization Cable Connection for Two Parallel Systems

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.