990-6139E-001

Connect the Power Cables

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the two indicated plates.

    Rear View 120-160 kVA 400 V/60-80 kVA 208 V UPS

    Rear View 200 kVA 400 V/100 kVA 208 V UPS

  3. In dual mains systems, remove the three single mains busbars.

    Rear View 120-160 kVA 400 V/60-80 kVA 208 V UPS

    Rear View 200 kVA 400 V/100 kVA 208 V UPS

  4. In TN-C systems only, rotate the jumper busbar to create a connection between the PE busbar and the neutral busbar.

    Rear View 120-160 kVA 400 V/60-80 kVA 208 V UPS

    Rear View 200 kVA 400 V/100 kVA 208 V UPS

  5. Route the power cables through the bottom of the UPS.
  6. Connect the PE cable to the PE terminal.

    Rear View 120-160 kVA 400 V/60-80 kVA 208 V UPS

    Rear View 200 kVA 400 V/100 kVA 208 V UPS

  7. Connect the input, output, and bypass (if applicable) cables.
  8. Connect the battery cables.
  9. Fasten the cables to the cable relief in the bottom of the UPS.
  10. Reinstall the two plates.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.