990-6139E-001

Route Signal Cables in a 200 kVA 400 V/100 kVA 208 V UPS

  1. Remove the top plate.
  2. Remove the plate in front of the gland plate.

    Rear View of the UPS

  3. Route the signal cables through the rear brush plate through the cable channel and to the communication interface on the front of the UPS.
  4. Reinstall the top plate.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.