990-6139E-001

Route Signal Cables in a 120-160 kVA 400 V/60-80 kVA 208 V UPS

  1. Remove the two covers in the left side.
  2. Route the signal cables through the bottom and to the communication interface. Fasten the cables to the cable reliefs.
  3. Reinstall the covers in the left side.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.