990-6139E-001

Recommended Bolts and Cable Lugs

Cable size (mm²) Bolt size Cable lug type
50 M8 KST TLK50-8
70 M10 KST TLK70-10
95 M10 KST TLK95–10
120 M10 KST TLK120–10
150 M10 KST TLK150–10
NOTE: If the recommended lug type is not available, use a local M8/M10 lug type as a substitute.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.