990-6139E-001

Connect the Parallel Cables in a Parallel System

  1. Connect the optional parallel cables between all the UPSs of the parallel system.
    NOTE: For location of parallel ports see Communication Interfaces.
  2. Verify the setting of the CAN_R (for location of CAN_R see Communication Interfaces).
    • For parallel systems with ≤ 4 parallel UPSs, CAN_R of all UPSs must be in ON position.
    • For parallel systems with ≥ 5 parallel UPSs, CAN_R of all UPSs must be in OFF position.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.