990-200001-001

Install the IP40 Kit (E3MOPT019) on a 120-160 kVA 400 V UPS for external batteries

NOTE: Rear access is required to install the IP40 kit on the UPS.
  1. Follow the UPS installation manual to install the UPS.
  2. Remove the upper and lower rear plates.

    Rear View of the UPS

  3. Install the provided IP40 frame from the IP40 kit with M4 screws.

    Rear View of the UPS

  4. Install the provided IP40 cover with M4 screws.

    Rear View of the UPS

  5. Reinstall the lower rear plate on the UPS. Alternatively, the lower rear plate can be reinstalled after the power cables have been connected.

    Rear View of the UPS

  6. Install M4 screws at the bottom of the IP40 frame.

    Rear View of the UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?