990-200001-001

Install the IP30 Kit (E3MOPT008) on a 60-80 kVA 400 V UPS with internal batteries

  1. Remove the rear gland plate and the rear brush plate from the UPS. Save the brush plate for reinstallation.

    Rear View of the UPS

  2. Remove the four rear plates. Discard the plates and save the screws.
  3. Install the four IP30 rear plates provided with the IP30 kit on the UPS. Reuse the screws from step 2. Alternatively, the two lowest IP30 rear plates can be installed after the power cables have been connected.

    Rear View of the UPS

  4. Reinstall the rear brush plate and the rear gland plate.
  5. Follow the UPS installation manual to install the UPS.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?