990-200001-001

Load Derating for UPS with IP30 Kit Installed

NOTICE
Risk of overheating
  • UPS with IP30 kit may have load deratings/temperature deratings.
Failure to follow these instructions can result in equipment damage.
UPS rating

Maximum continuous load at 30 °C at power factor = 1

Maximum continuous load at 35 °C at power factor = 1

Maximum continuous load at 40 °C at power factor = 1

60 kVA

60 kVA

55.5 kVA

51 kVA

80 kVA

80 kVA

74 kVA

68 kVA

100 kVA

100 kVA

92.5 kVA

85 kVA

120 kVA

120 kVA

111 kVA

102 kVA

160 kVA

160 kVA

148 kVA

136 kVA

200 kVA

200 kVA

185 kVA

170 kVA

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?