990-200001-001

Install the IPX2 Kit (E3MOPT014) on a 60-100 kVA 400 V UPS for external batteries

NOTE: Top access is required to install the IPX2 kit on the UPS.
  1. Follow the UPS installation manual to install the UPS.
  2. Remove the top panel.
  3. Install the new IPX2 top plate from the IPX2 kit with M4 screws.
  4. Install the provided IPX2 top cover on the top plate with M6 screws and nylon washers.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?