990-200001-001

Load Derating for UPS with IP40 Kit Installed

NOTICE
Risk of overheating
  • UPS with IP40 kit may have load deratings/temperature deratings.
Failure to follow these instructions can result in equipment damage.
UPS rating

Maximum continuous load at 30 °C at power factor = 1

Maximum continuous load at 40 °C at power factor = 1

60 kVA

48 kVA

45 kVA

80 kVA

64 kVA

60 kVA

100 kVA

80 kVA

75 kVA

120 kVA

96 kVA

90 kVA

160 kVA

128 kVA

120 kVA

200 kVA

160 kVA

150 kVA

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?