990-200001-001

Install the IP30 Kit (E3MOPT009) on a 60-100 kVA 400 V UPS for external batteries

  1. Remove the lower rear plate from the UPS. Save for reinstallation.

    Rear View of the UPS

  2. Remove the upper rear plate from the UPS. Discard the upper rear plate and save the screws.
  3. Install the new upper IP30 rear plate provided with the IP30 kit on the UPS. Reuse the screws from step 2.

    Rear View of the UPS

  4. Reinstall the lower rear plate on the UPS. Alternatively, the lower rear plate can be installed after the power cables have been connected.
  5. Follow the UPS installation manual to install the UPS.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?