ELKO - Smart Tag_WH_00

Advanced settings

Advanced settings is applicable for Grid, Solar, Solar / Battery (combo) to re-configure the power direction.
The following is an example of configuring the Advance settings for Grid in any one of the following scenarios:
  • Installed a new On Grid solar system.

  • Removed the On Grid solar system.

  • If power direction is incorrect with the existing On Grid solar system.

  • If you have changed your Grid limit (power contract) .

  1. On the Home screen, tap > Devices > Energy > Grid > Advance settings.
  2. Tap OK when the caution window is prompted for confirmation.
  3. Follow any one of these steps based on the requirement:
    • If you have installed a new On Grid solar system. Refer to Pairing the device with an On Grid solar system.
    • If you have removed the solar system, tap (A) and select No.
      NOTE: If you have configured your SmartTag as Solar or Solar / Battery (combo), (A) field Do you have solar panels? will be disabled. Refer to Pairing the device with ESS.
    • If your solar system feed only the Grid, tap (B) and select Yes, I sell all of it.
    • To update your power contract, select your grid limit (kVA/A/kW) (C) from the dropdown menu, then tap and enter a value using the dial pad as per your country.
    • Enable or disable the Reverse Direction (D) toggle switch, if the power direction is incorrect with the existing On Grid solar system. Refer to Pairing the device with an On Grid solar system.
    TIP: During night time, the power direction must be from Grid to Home, if the power direction is incorrect enable or disable the Reverse Direction (D) toggle switch accordingly.

    Follow the same procedure to configure the Advance settings for ESS -Solar, Solar / Battery (combo) .

    1. On the Home screen, tap > Devices > Energy > Solar > Advance settings.

    2. Enable or disable the Reverse Direction (D) if the power direction is incorrect with the existing ESS. Refer to Pairing the device with Energy storage system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?