ELKO - Smart Tag_WH_00

Installing the device

It is recommended to install the Smart Tag within 3 meters of the Wiser Hub for best results. This provides a good a network signal strength and helps to prevent online/offline issues, which might result in corrupting data. The signal quality is best maintained when there are no big obstructions (for example thick walls, metal cabinets, etc.) between the Smart Tag & Wiser Hub. Refer to the installation instruction supplied with this product.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?