ELKO - Smart Tag_WH_00

Identifying the device

Using the Wiser Home app, you can identify the device.
  1. On the Home screen, tap .
  2. Tap Devices and select the required SmartTag from the list and then tap Identify (A).
    A notification window is prompted and the status LED flashes green for 30 seconds on the SmartTag.
  3. Tap OK on the notification window when you have finished identifying the SmartTag.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?