ELKO - Smart Tag_WH_00

History

On the History page, you can choose to filter the data by Energy sources or Load consumption and select a time frame according to your preference. The app automatically saves your filter preferences and applies them automatically in future sessions.

History of Grid import:
  1. On the bottom navigation bar, tap > History.

  2. On the History page, select a required time frame (A):

    • Hours

    • Days

    • Months

    • Years


History of Grid import and export:
IMPORTANT: Applicable only for Grid with an existing On Grid solar system.
  1. On the History page, select a required time frame (A):

    NOTE: The Grid import is shown in blue and the excess energy of solar production sold is shown in green.


History of load consumption
IMPORTANT: You can view the power consumed by individual loads only if you have installed additional SmartTag for them.
  1. On the History page, tap and select Load consumption.

  2. Tap (A) and select a required time frame.

History of Solar and Battery
IMPORTANT: You can view the history of solar and battery only if you have installed additional SmartTag for them.
  1. On the History page, select a required time frame (A).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?