ELKO - Smart Water Heater Puck_WH_00

LED Indications

Pairing

User Action

LED Indication

Status

Press the Setup/Reset button 3 times

Status LED blinks yellow, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, status LED glows green for some time before turning Off.

Resetting

User Action

LED Indication

Status

Press the Setup/Reset button 3 times and hold it for > 10 s.

After 10 s, status LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the status LED starts blinking green before turning Off.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.