ELKO - Smart Water Heater Puck_WH_00

Removing the device

Using the Wiser Home app, you can remove the module from the system.
To remove the device:
  1. On the Home screen, tap .
  2. Tap Devices > Power Micromodule > Delete (A).
  3. Tap Remove from System.
    Removing the device will delete all the historical data.
    NOTE:
    • Removing the device will reset the module. After reset the LED turns amber indicating that the module is ready to pair with another network.

    • If there is a problem while pairing or resetting the module, refer to .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.