ELKO - Smart Water Heater Puck_WH_00

About the device

The Smart Water Heater Puck (hereinafter referred to Water Heater/Puck) is intended for switching loads (up to 3000 W) such as a hot water tank or a socket outlet. In combination with the Wiser Home app, the energy consumption can be measured and if necessary the load can be shed. Automatic module switch-off in case of load shedding or demand response request as well. Up to 10 modules can be added to the same system.

Operating elements:

  1. Status LED

  2. Setup/Reset button

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.