ELKO - Smart Water Heater Puck_WH_00

Wiser Home AI

Using the Wiser Home app, you can view how the devices are controlled and scheduled for usage.

The Wiser Home AI feature automatically schedules your high-consuming devices to run during the cheapest electricity rates, helping to lower your energy bill. By enrolling devices like EV chargers or resistive water boilers, this feature shifts loads to low-tariff periods. It also helps the EV chargers to consume the excessive solar energy production. It works with variable tariffs, such as peak/off-peak rates, and requires users to answer routine questions.

For more information on Wiser Home AI refer to the respective System User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.