ELKO - Smart Water Heater Puck_WH_00

Changing Nominal Power

Nominal Power is the maximum power this device can manage. By default, the value is 2000 W. Using the Wiser Home app you can change the value if required.
To change the Nominal Power value:
  1. On the Home screen, tap .
  2. Tap Devices > Climate > Power Micromodule > Nominal Power (A).

  3. Tap OK and enter a value between 0 to 3000 W.
    The settings will be saved automatically.
    NOTE: The Nominal power value will only be used for the future updates in the Wiser Home app.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.