SUG_NO_WH-01

Away Mode

The Away Mode is designed to set your home in a sensible state when you are away for longer periods (e.g. being away for the weekend). It temporarily overrides the normal controls (e.g. moments, automation) implemented in the hub. When you disable away mode, the controls revert to the state they where prior to activating the Away mode.

By default, the Heating setpoint is 16 °C, and the Cooling setpoint is Off.

You can change the target temperature and adjust device behaviors (turn off lights, close shutters etc.) for Away Mode.

Set the Device State / Temperature Setpoint in Away Mode:

  1. On the Home screen, tap > Away Mode.

  2. Tap the toggle switch to enable or disable the device when in away mode. Tap to modify the heating and cooling setpoints.

Enable/Disable Away Mode

  1. On the Home screen, tap Automation .

  2. Enable/Disable the toggle switch to activate or deactivate the away mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.