SUG_NO_WH-01

Shutter

SmartBlinds Push

EKO09692

EKO09694

EKO09695

EKO09691

Remotely open/close shutters, or automatically set shutter position in response to a specified condition or event.

Instruction Sheet (PDF)

Device User Guide

SmartBlinds Puck

EKO07145

Combine the advantages of smart shutter functionality with ordinary mechanical push-button switches. Up to 10 mechanical push-button switches can be connected to one SmartBlinds Puck to control a connected shutter.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.