SUG_NO_WH-01

Climate

Smart Radiator Thermostat

EKO09765

The Smart Radiator Thermostat uses integrated temperature sensors to control the flow of water through a radiator, thereby regulating the temperature in a room. The target temperature and switching times are set in the Wiser Home App.

Instruction Sheet (PDF)

Device User Guide

Smart ZB Thermostat 16 A

EKO07258

EKO07257

EKO07254

EKO07259

EKO30465

The Smart ZB Thermostat 16 A is mainly used for electrical heating applications like electrical underfloor heating and electrical radiators / heating panels.

Instruction Sheet (PDF)

Device User Guide

Wiser Room Thermostat with display

CCTFR6400
CCTFR6401

Wireless, battery-powered, colored touch-button display to set the room temperature.

Instruction Sheet (PDF)

Device User Guide

Wiser Underfloor Heating Connection Strip

CCTFR6600
CCTFR6610
CCTFR6620

Control thermal actuator valve heads to regulate the flow of hot water in the underfloor pipes.

Instruction Sheet (PDF)

Device User Guide

Wiser 16 A Relay for Temperature Control

CCTFR6700

Control electrical heaters with On/Off commands (Relay output) or Fil Pilote commands.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.