SUG_NO_WH-01

History

Provides history of power consumed by loads. If there is an existing On Grid solar system, the app provides history of imported and exported energy.

  1. On the page, tap History.

  2. You can change the displayed timeframe (hours, days, months and years), by tapping (A).

    NOTE: The Grid import is shown in blue and the excess energy of solar and battery is shown in green.

  3. You can tap and select Load consumption to view the energy consumed by individual loads.

  4. Tap (A) and select a required time frame.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?