SUG_NO_WH-01

Compatible Wiser Devices for Matter Bridge

Following are the Matter bridge compatible devices:

Refer to List of Wiser Devices for the links to Device user guide for each devices.

Sensors

SmartSensor Door/Win Wireless

SmartSensor Leakage Wireless

SmartSensor PIR Wireless

SmartSensor Climate Wireless

Dimmers

SmartDim LED Puck Multiwire

Shutters

SmartBlinds Puck
SmartBlinds Push

Appliances

SmartPlug 16A

SmartSwitch Push Wireless Plus
SmartSocket Double 16A
SmartSocket Single 16A

Climate

Wiser Underfloor Heating Connection Strip

Wiser 16 A Relay for Temperature Control

Wiser Room Thermostat

Smart Radiator Thermostat

Safety

Wiser Smoke Alarm - Battery

Wiser Smoke Alarm 230 V

Energy

Smart Tag Energy

PowerTag C

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.