SUG_NO_WH-01

Energy Domain without Grid

You can monitor your energy consumption and production even without a grid monitoring device (PowerTag E). If standalone energy devices are installed in your home, the Energy Centre will be available to help you manage and monitor your energy usage.

Standalone Energy Devices:

  • Schneider Charge

  • Wiser 16 A Relay for Temperature Control

  • Smart Water Heater Puck

  • Connected Sockets

  • Smart Tag Energy

  • SmartPlug 16A

In the Energy Centre, you can monitor your energy production, view detailed consumption history, and track energy costs by entering your tariff.

IMPORTANT: The Wiser system supports the configuration with the following energy source and combinations:
  • No Sources

  • Solar

  • Solar + Battery

To navigate to the Energy Centre:

  1. On the Home Screen, tap .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.