SUG_NO_WH-01

Safety & Security

Smart Smoke Alarm Battery

EKO09761

The Smart Smoke alarm battery uses a photoelectric sensor to detect smoke generated by fire. It also includes a temperature sensor that detects heat by rapid increase in temperature. When connected to the system, the device will send the notifications via the Wiser Home app.

Instruction Sheet (PDF)

Device User Guide

Smart Smoke Alarm 230 V

EKO09764

The Smart Smoke Alarm 230 V uses a photoelectric sensor to detect smoke generated by fire and a temperature sensor that detects heat caused by rapid increase in temperature. It also includes a backup battery that allows the device to work if the power supply is disconnected. When connected to the system, the device will send notifications via the Wiser Home app.

Instruction Sheet (PDF)

Device User Guide

SmartSensor Climate Wireless

EKO07219

Maintains a comfortable environment in the home by detecting changes in temperature and humidity and reporting climate data to the hub

Instruction Sheet (PDF)

Device User Guide

SmartSensor Leakage Wireless

EKO07218

Detects the presence of water, and alert via an alarm and/or notification.

Instruction Sheet (PDF)

Device User Guide

SmartSensor Door/Win Wireless

EKO07217

Detects when windows or doors are opened or closed and send the status to the hub.

Instruction Sheet (PDF)

Device User Guide

SmartSensor PIR Wireless

EKO07220

Reports the detection of movement and measures the luminance of the environment.

Instruction Sheet (PDF)

Device User Guide

Motion Sensor Outdoor, 360

EKO025212

EKO025213

It offers advanced motion detection, LUX measurement, and temperature sensing capabilities. It allows you to automate and enhance your smart home environment effortlessly.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.