SUG_NO_WH-01

Insights

The Insights provides an overview of your energy usage, savings, and patterns that impact your energy efficiency.

  1. From the Home screen, tap .

    B

    Shows the percentage of energy saved for the current month, along with a 3-month average comparison. It also provides data on hours saved in Away Mode and allows you to enable Eco Mode for additional savings.

    C

    Tracks adjustments made to heating, including the number of times the heating was turned up or down, as well as environmental factors like hours of sunshine, which may impact energy needs. Refer to Weather and Heating for detailed information.

    D

    A graph shows how external temperatures have affected heating usage over the past 30 days. Tap Heat Report to view temperature data for each room in your home. Refer to Heat report for detailed information.

    NOTE: B, C, and D will not appear if you do not have heating devices installed at your home.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.