Schneider Electric Green Premium ™ Ecolabel
Description
Green Premium by Schneider Electric is a label that allows you to develop and promote an environmental policy while preserving your business efficiency. This ecolabel is compliant with up-to-date environmental regulations.
Accessing Green Premium
Green Premium data on labeled products can be accessed online through any of the following ways:
Checking Products Through the Schneider Electric Website
To check the environmental criteria of a product using a PC or smartphone, follow these steps:
Step |
Action |
---|---|
1 |
From www.se.com, select . |
2 |
Click to open the search tool webpage. |
3 |
Fill in the fields:
|
4 |
To search for several products simultaneously, click the button, and then fill in the fields. |
5 |
Click to generate a report of the environmental criteria available for the products with the entered commercial references. |
Environmental Criteria
The Green Premium ecolabel provides documentation on the following criteria about the environmental impact of the products:
-
RoHs: European Union Restriction of Hazardous Substances (RoHS) directive.
-
REACh: European Union Registration, Evaluation, Authorization, and Restriction of Chemicals regulation.
-
PEP: Product Environmental Profile.
-
EoLI: End of Life Instructions.
@Writer (07/2016): for translation phase, provide the French translator with the corresponding page of the Masterpact MTZ Catalogue in French.
RoHs
Schneider Electric products are subject to RoHS requirements at a worldwide level, even for the many products that are not required to comply with the terms of the regulation. Compliance certificates are available for products that fulfill the criteria of this European initiative, which aims to eliminate hazardous substances.
REACh
Schneider Electric applies the strict REACh regulation on its products at a worldwide level, and discloses extensive information concerning the presence of SVHC (Substances of Very High Concern) in all of these products.
PEP
Schneider Electric publishes complete set of environmental data, including carbon footprint and energy consumption data for each of the life cycle phases on all of its products, in compliance with the ISO 14025 PEP ecopassport program. PEP is especially useful for monitoring, controlling, saving energy, and/or reducing carbon emissions.
EoLI
These instructions provide:
-
Recyclability rates for Schneider Electric products.
-
Guidance to mitigate personnel hazards during the dismantling of products and before recycling operations.
-
Part identification for recycling or for selective treatment, to mitigate environmental hazards/incompatibility with standard recycling processes.
Info. to experts (11/2016): This map content is present in Masterpact MTZ1 User Guide (Schneider products Green Premium), Masterpact MTZ2/3 User Guide (Schneider products Green Premium), Masterpact MTZ Maintenance Procedures Levels Basic and Advanced (Introduction), Masterpact MTZ Maintenance Procedures Level Exclusive (Introduction), Masterpact MTZ Internal Maintenance Procedures (Introduction), IFE Modbus (Presentation), EIFE (Presentation) and Input/Output LV Circuit Breaker (Troubleshooting). Any changes made will be made in all these guides.