DOCA0155EN-12

Procedure for Finding the Firmware Version of a MicroLogic Active Control Unit

Follow this procedure to find the firmware version of a MicroLogic Active control unit:

Step Action

1

Connect a PC running EcoStruxure Power Commission software to the MicroLogic Active control unit.

A Cable plug connected to the USB-C port of MicroLogic Active control unit

B USB-A to USB-C port cable

C PC running EcoStruxure Power Commission software

2

Launch EcoStruxure Power Commission software.

3

From the EcoStruxure Power Commission home page, click the Circuit Breaker section.

4

Click CONNECT on the displayed pop-up screen, to add the device to the switchboard and connect to it.

Result: A window displays to indicate that device connection is in progress. It disappears automatically when the device is connected.

5

Enter the account details when prompted.

6

Click Firmware.

The firmware version of the MicroLogic Active control unit is displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?