DOCA0155EN-15

Firmware Update with EcoStruxure Power Commission Software

Use the latest version of EcoStruxure Power Commission software:

  • To check the firmware compatibility of the devices in the Intelligent Modular Unit (IMU).

  • To find the firmware version of a MicroLogic trip unit or control unit (refer to the following procedure).

  • To update the devices with the latest firmware version available.

Click here to download the latest version of EcoStruxure Power Commission software.

For more information about the use of EcoStruxure Power Commission software, refer to EcoStruxure Power Commission Online Help available in the software.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.