Enerlin'X Devices Compatible with NT/NW MicroLogic A/E
Compatibility with Enerlin'X devices of the IMU depends on the firmware version of the BCM ULP module only. It does not depend on the firmware version of the MicroLogic trip unit. For more information, refer to DOCA0152EN BCM ULP - Firmware Release Notes .
| NOTICE |
|---|
|
HAZARD OF NON-COMMUNICATION BETWEEN the IMU DEVICES
Check the firmware compatibility of the devices in the
IMU by using the latest version of EcoStruxure Power
Commission software, and follow the recommended actions.
Failure to follow these instructions can result in critical
firmware discrepancy.
|
The following table shows the minimum firmware version of Enerlin'X devices that is required to enable communication with a BCM ULP module.
| Device | Part number | Firmware version of BCM ULP module | |
|---|---|---|---|
| 3.3.4 – 4.0.6 | ≥ 4.0.7 | ||
|
IFM Modbus-SL interface for one circuit breaker with RJ45 |
LV434000 |
– |
≥ 003.000.012 |
|
IFM Modbus-SL interface for one circuit breaker |
TRV00210 STRV00210 |
– |
≥ 002.002.007 |
|
IFE Ethernet interface for one circuit breaker with RTC |
LV434001 |
– |
≥ 003.006.011 |
|
IFE Ethernet interface for one circuit breaker |
LV434010 |
– |
|
|
IFE Ethernet switchboard server with RTC |
LV434002 |
– |
≥ 003.006.011 |
|
IFE Ethernet switchboard server |
LV434011 |
– |
|
|
IO input/output application module for one circuit breaker |
LV434063 |
– |
≥ 002.001.004 |
|
FDM121 front display module for one circuit breaker |
TRV00121 STRV00121 |
≥ 002.003.004 |
≥ 002.003.005 |
|
FDM128 Ethernet display for eight devices |
LV434128 |
– |
≥ 5.5.8 |
|
USB maintenance module |
TRV00911 |
≥ 001.000.009 |
≥ 001.000.009 |
Example: An NT/NW MicroLogic A trip unit equipped with a BCM ULP circuit breaker communication module with firmware version 3.3.4 is compatible with:
-
FDM121 display with firmware version greater than or equal to 002.003.004
-
USB maintenance module with firmware version greater than or equal to 001.000.009
The firmware version of the BCM ULP module must be updated to a version greater than 4.0.7 to be compatible with IO module or IFE interfaces. Use EcoStruxure Power Commission software to update the firmware of the BCM ULP module.