DOCA0155EN-15

NT/NW MicroLogic E Firmware History

NT/NW MicroLogic E trip units are designed for:

  • MasterPacT NT/NW circuit breakers

  • ComPacT NS630b-3200 circuit breakers

NOTE: The information related to the new generation of MicroLogic E trip units for ComPacT NS circuit breakers in this document applies also to MicroLogic E trip units for ComPact NS circuit breakers. The exceptions are mentioned wherever applicable.
Date NT/NW MicroLogic E firmware version Availability
June 2013 1.016 Release for manufacturing
June 2012 1.013 Obsolete
October 2011 1.012 Obsolete
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?