Digital Modules Compatible with MTZ MicroLogic X Control Unit
The following table presents the minimum MicroLogic X firmware version needed for the Digital Module to function:
| Digital Module | Part number | Firmware version of MTZ MicroLogic X control unit |
|---|---|---|
|
IDMT ground-fault protection |
LV850038 |
≥ 005.103.000 |
|
IEC 61850 for MasterPacT MTZ |
LV850046 |
≥ 004.101.000 |
|
Directional overcurrent protection |
LV850015 |
≥ 004.101.000 |
|
IDMTL overcurrent protection |
LV850037 |
≥ 004.101.000 |
|
Under/Overfrequency protection |
LV850013 |
≥ 003.012.000 |
|
Individual harmonics analysis |
LV850006 |
≥ 002.000.002 |
|
Under/Over voltage protection |
LV850012 |
≥ 002.000.002 |
|
Reverse active power |
LV850011 |
≥ 002.000.002 |
|
Ground-fault alarm |
LV850007 |
≥ 002.000.002 |
|
Energy Reduction Maintenance Settings (ERMS) |
LV850009 |
≥ 002.000.002 |
|
Modbus legacy dataset |
LV850045 |
≥ 002.000.002 |
|
Energy per phase |
LV850002 |
≥ 001.000.002 |
|
Power restoration assistant |
LV850004 |
≥ 001.000.002 |
|
MasterPacT operation assistant |
LV850005 |
≥ 001.000.002 |
|
Waveform capture on trip event |
LV850003 |
≥ 001.000.002 |
Refer to DOCA0102EN MasterPacT MTZ - MicroLogic X Control Unit - User Guide for compatibility of the Digital Module with Enerlin'X devices.