NSX MicroLogic 5/6 Firmware History
The new generation of NSX MicroLogic 5/6 trip units is designed for:
-
ComPacT NSX circuit breakers
-
PowerPacT H-, J-, and L-frame circuit breakers
Each hardware version of an NSX MicroLogic 5/6 trip unit is compatible with one or more firmware versions (see table below). You can update an NSX MicroLogic 5/6 trip unit to the latest firmware version compatible with its hardware. For more information, refer to DOCA0153EN ComPacT NSX - MicroLogic 5/6 Trip Unit - Firmware Release Notes.
| Date | NSX MicroLogic 5/6 hardware version | NSX MicroLogic 5/6 firmware version | Availability |
|---|---|---|---|
|
October 2025 |
HW 001.000.000 |
FW 001.008.004 |
Release for manufacturing |
|
March 2024 |
HW 001.000.000 |
FW 001.008.003 |
Obsolete |
|
January 2022 |
HW 001.000.000 |
FW 001.006.001 |
Obsolete |
|
July 2021 |
HW 001.000.000 |
FW 001.005.002 |
Obsolete |
|
April 2021 |
HW 001.000.000 |
FW 001.005.001 |
Obsolete |
|
June 2018 |
HW 001.000.000 |
FW 001.003.000 |
Obsolete |
|
December 2016 |
HW 001.000.000 |
FW 001.002.002 |
Obsolete |
|
December 2015 |
HW 15* |
FW 1.1.0 |
Obsolete |
|
December 2014 |
HW 15 |
FW 1.0.3 |
Obsolete |
|
July 2008 |
HW 15 |
FW 1.0.2 |
Obsolete |
Example: MicroLogic 5 trip unit with firmware version 001.002.002 can be updated to firmware version 001.008.003, which is compatible with hardware version 001.000.000. The firmware of NSX MicroLogic 5/6 trip units with hardware version 15 or 15* cannot be updated.