Enerlin'X Devices Compatible with NSX MicroLogic 7 Trip Units
| NOTICE |
|---|
|
HAZARD OF NON-COMMUNICATION BETWEEN the IMU DEVICES
Check the firmware compatibility of the devices in the
IMU by using the latest version of EcoStruxure Power
Commission software, and follow the recommended actions.
Failure to follow these instructions can result in critical
firmware discrepancy.
|
The following table shows the minimum firmware version of Enerlin'X devices that is required to enable communication with an NSX MicroLogic 7 trip unit.
| Device | Part number | Firmware version of NSX MicroLogic 7 trip unit |
|---|---|---|
| ≥ 002.001.001 | ||
|
IFM Modbus-SL interface for one circuit breaker with RJ45 |
LV434000 |
≥ 003.000.012 |
|
IFM Modbus-SL interface for one circuit breaker |
TRV00210 STRV00210 |
≥ 002.002.007 |
|
IFE Ethernet interface for one circuit breaker with RTC |
LV434001 |
≥ 003.006.011 |
|
IFE Ethernet interface for one circuit breaker |
LV434010 |
|
|
IFE Ethernet switchboard server with RTC |
LV434002 |
≥ 003.006.011 |
|
IFE Ethernet switchboard server |
LV434011 |
|
|
IO input/output application module for one circuit breaker |
LV434063 |
≥ 002.001.004 |
|
FDM121 front display module for one circuit breaker |
TRV00121 STRV00121 |
≥ 002.003.005 |
|
FDM128 Ethernet display for eight devices |
LV434128 |
≥ 5.5.6 |
|
USB maintenance module |
TRV00911 |
≥ 001.000.009 |
|
BSCM Modbus SL/ULP module |
LV434220 S434220 |
≥ 001.000.000 |
|
BSCM circuit breaker status control module |
LV434205 |
≥ 002.002.007 |