DOCA0155EN-13

MTZ MicroLogic X Firmware History

MTZ MicroLogic X control units are designed for:

  • MasterPacT MTZ1 circuit breakers

  • MasterPacT MTZ2/MTZ3 circuit breakers

Date MicroLogic X Firmware version Availability

February 2024

005.103.003

Release for manufacturing

February 2023

005.103.003

Digital release in EcoStruxure Power Commission (EPC) software

October 2021

004.109.000

Obsolete

March 2021

004.107.000

Obsolete

October 2020

004.105.003

Obsolete

April 2020

004.105.000

Obsolete

December 2019

004.101.000

Obsolete

July 2019

003.012.000

Obsolete

March 2019

003.011.000

Obsolete

November 2018

002.000.004

Obsolete

April 2018

002.000.003

Obsolete

March 2018

002.000.002

Obsolete

December 2017

001.000.206

Obsolete

July 2017

001.000.202

Obsolete

December 2016

001.000.200

Obsolete

NOTE: This firmware history also applies to MicroLogic Xi control units. A MicroLogic Xi control unit is a MicroLogic X control unit without Bluetooth® Low Energy communication. The firmware versions of the MicroLogic X and MicroLogic Xi control units are the same from firmware version 004.105.003.

For more information, refer to DOCA0144EN MasterPacT MTZ - MicroLogic X Control Unit - Firmware Release Notes .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?