DOCA0155EN-11

Enerlin'X Devices Compatible with MTZ MicroLogic X Control Unit

NOTICE
HAZARD OF NON-COMMUNICATION BETWEEN the IMU DEVICES
Check the firmware compatibility of the devices in the IMU by using the latest version of EcoStruxure Power Commission software, and follow the recommended actions.
Failure to follow these instructions can result in critical firmware discrepancy.

The following table shows the minimum firmware version of Enerlin'X devices that is required to enable communication with an MTZ MicroLogic X control unit.

Device Part number Firmware version of MTZ MicroLogic X control unit
001.000.200 to 001.000.206 ≥ 002.000.002

IFM Modbus-SL interface for one circuit breaker with RJ45

LV434000

≥ 003.000.012

released version > 003.001.000

IFM Modbus-SL interface for one circuit breaker

TRV00210

STRV00210

IFE Ethernet interface for one circuit breaker with RTC

LV434001

≥ 003.007.024

IFE Ethernet interface for one circuit breaker

LV434010

≥ 003.005.003 and date code ≥ HL16485 (1)

≥ 003.007.024

IFE Ethernet switchboard server with RTC

LV434002

≥ 003.007.024

IFE Ethernet switchboard server

LV434011

≥ 003.005.003 and date code ≥ HL16485 (1)

≥ 003.007.024

EIFE Embedded Ethernet interface for one MasterPact MTZ drawout circuit breaker

LV851001

≥ 003.005.003

≥ 003.007.024

IO input/output application module for one circuit breaker

LV434063

≥ 003.002.002 and date code ≥ HL16486 (2)

≥  003.003.011

FDM121 front display module for one circuit breaker

TRV00121

STRV00121

≥ 004.000.009

≥ 004.000.009

FDM128 Ethernet display for eight devices

LV434128

≥ 6.3.4

≥ 6.5.3

(1) IFE hardware is compatible if manufacturing date code on the IFE label is greater than HL16485. IFE hardware with manufacturing date code lower than HL16485 operates correctly but generates a non-critical hardware discrepancy.

(2) IO module hardware is compatible if manufacturing date code on the IO module label is greater than HL16486. IO module hardware with manufacturing date code lower than HL16486 operates correctly but generates a non-critical hardware discrepancy.

Example: An MTZ MicroLogic X control unit with firmware version  001.000.200 is compatible with:

  • IFM interface LV434000 with firmware version greater than or equal to 003.000.012

  • IFE interface with firmware version greater than or equal to 003.005.003 and date code greater than or equal to HL16485

  • EIFE interface with firmware version greater than or equal to 003.005.003

  • IO module for one circuit breaker with firmware version 003.002.002 and date code greater than or equal to HL16486

  • FDM128 display with firmware version greater than or equal to 6.3.4

The MTZ MicroLogic X control unit must be updated to firmware version greater than or equal to 002.000.002 to be compatible with an IFE interface with RTC.

NOTE: To benefit from the latest IMU features, it is recommended to update the firmware of the MTZ MicroLogic X control unit and the Enerlin'X devices of the IMU.

QR code for this page

Was this helpful?