990-6470B-012

Caractéristiques du couple de serrage

Taille de vis Couple
M6 5 Nm
M8 17,5 Nm
M10 30 Nm
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Contenu utile ?