990-91377J-001

Batteries

Common Battery

For parallel UPS systems, simplified common battery configuration (VRLA/Lithium-ion) is supported.

End of Discharge Voltage

The voltage is 1.6 to 1.75 per cell depending on discharge ratio.

Standard VRLA Voltage Levels

NOTE: Specific configurations may differ from the general constraint shown above.

Battery Runtimes

Go to www.se.com for battery runtimes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.