990-91377J-001

Leakage Current

380/400/415 V UPS System 4-wire Installation at 100% Load

UPS rating Leakage current
200 kW-500 kW 700 mA
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.